Performance of rtsp server streaming with L4.1.15 on i.MX6 Dual

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Performance of rtsp server streaming with L4.1.15 on i.MX6 Dual

761 Views
letan
Contributor III

Hello,

I have just upgrade up to L4.1.15 with imx-vpu-5.4.33 for our custom board(i.MX6 Dual).

Then the performance of the streaming is ~30fps without encryption. But actually when we run the streaming with libsrtp 1.5.3 and openssl encryption-enabled, the performance of the streaming downs to ~25-26fps.

Could you all please help me to clarify the problem?

Regards,

Tan

Labels (3)
2 Replies

601 Views
jamesbone
NXP TechSupport
NXP TechSupport

In order to use OpenSSL engine, some changes should be provided in libsrtp.

Hope the following helps.

libsrtp / Mailing Lists

0 Kudos
Reply

601 Views
letan
Contributor III

That changes has already been there on openssl version 1.0.2. But how we know whether we are using hardware cryptodev while streaming or not?