Pcie issue of the IMX6D processor

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Pcie issue of the IMX6D processor

980件の閲覧回数
lorinwang
Contributor I

Hi, all,

    I am working on a PAD which to use the IMX6D processor.  There is a wifi module which a PCIe interface connected to mini PCIe interface of the IMX6D. The system was crash every several hours when the wifi module connected to main board. The system didn't crash if don't to connect the wifi module. I have check the power of the system and it no problem.  Does anyone see this issue or the similar issues? How solve this issue? Thanks.

ラベル(2)
0 件の賞賛
返信
1 返信

864件の閲覧回数
richard_zhu
NXP Employee
NXP Employee

Hi
What's kind of crash it is?

intel iwl4965,5100,6200,6300 had been verified on imx6 reference boards, no such kind of problem.

Best Regards

Richard.

0 件の賞賛
返信