Patches for u-boot lf_v2022.04

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Patches for u-boot lf_v2022.04

1,092件の閲覧回数
jo-so-nx
Contributor II

I've two patches for branch lf_v2022.04 of u-boot and I found no other place to submit them. Please let me know if I should submit them somewhere else, or if they are wrong.

 

Unfortunately, the second patch isn't accepted as attachment. So here it is inline:

From: =?UTF-8?q?J=C3=B6rg=20Sommer?= <joerg.sommer@navimatix.de>
Date: Mon, 2 Oct 2023 16:05:28 +0200
Subject: [PATCH 2/2] imx8m_hdmi: shrink white space to help dtoc
 
When enabling `CONFIG_SPL_OF_PLATDATA` the build fails with:
 
    ValueError: drivers/video/nxp/imx/hdmi/imx8m_hdmi.c: Unknown compatible var 'imx8m_hdmi_ids' (found:  imx8m_hdmi_ids)
---
 drivers/video/nxp/imx/hdmi/imx8m_hdmi.c | 2 +-
 1 file changed, 1 insertion(+), 1 deletion(-)
 
diff --git a/drivers/video/nxp/imx/hdmi/imx8m_hdmi.c b/drivers/video/nxp/imx/hdmi/imx8m_hdmi.c
index fb069d2ed57..f1e38082515 100644
--- a/drivers/video/nxp/imx/hdmi/imx8m_hdmi.c
+++ b/drivers/video/nxp/imx/hdmi/imx8m_hdmi.c
@@ -293,7 +293,7 @@ struct dm_display_ops imx8m_hdmi_ops = {
        .enable =  imx8m_hdmi_enable,
 };
 
-static const struct udevice_id  imx8m_hdmi_ids[] = {
+static const struct udevice_id imx8m_hdmi_ids[] = {
        { .compatible = "fsl,imx8mq-hdmi" },
        { }
 };
0 件の賞賛
返信
3 返答(返信)

1,057件の閲覧回数
jo-so-nx
Contributor II

Hi @Chavira, thank you for your reply.

 

I'm configuring U-Boot for our device and I came across these minor problems. I found no other place to submit patches. Only other posts in the community they suggested to send them here and someone from NXP would pick them up and forward them.

I would also like to here some feedback, if they are the right or wrong approach.

 

Kind regards Jörg

0 件の賞賛
返信

1,047件の閲覧回数
Chavira
NXP TechSupport
NXP TechSupport

Hi @jo-so-nx!

Are you using an EVK board?

What processor are you using?

Can you tell me more about the problem?

Best Regards!
Chavira

0 件の賞賛
返信

1,071件の閲覧回数
Chavira
NXP TechSupport
NXP TechSupport

Hi @jo-so-nx!
Thank you for contacting NXP Support!

Do you want to send the patches to something in particular?

Do you have a previous case?

Best Regards!
Chavira

0 件の賞賛
返信