Patches for L5.0.0

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Patches for L5.0.0

1,062 Views
donfreiling
Contributor III

I've just followed the instructions in Android User's Guide Rev. L5.0.0_1.0.0-ga to get and patch the Android BSP, kernel and u-boot code and I'm ready to build for SDP.

One question: There are several patch files on the Freescale site for the IMX6 (see below). Have these already been incorporated in to the android_L5.0.0_1.0.0-ga_core_source patches or do I need to apply them as well?


Thanks!

Don

IMX6_DQ_SDX_SD_DEMO_IMAGE_PATCH​​ (REV R13.4)

by FREESCALE

Source code patches needed to create the SD card demo images provided with the i.MX 6Quad SDP and SDB boards. The patches are only needed on the...

  • Date : 12/10/2012
  • Format : gz
  • Size : 6K

IMX6_R13.4.1.02_ANDROID_PATCH (REV 13.4.1.02)

by FREESCALE
Android 13.4.1.02 patch release supports to run i.MX 6Solo emulation on i.MX 6DualLite SABRE-SD platform. Patch based on Android 13.4.1 BSP. Includes...
  • Date : 1/30/2013
  • Format : gz
  • Size : 59690K
Download

IMX6_R13.41_ANDROID_PATCHES (REV R13.4.1)

by FREESCALE
Add-on patches to resolve issues in i.MX 6Quad, i.MX 6Dual, and i.MX 6DualLite Android 13.4.1 BSP.
  • Date : 12/12/2012
  • Format : gz
  • Size : 3K
Download

IMX6_R13.4_ANDROID_PATCHES (REV R13.4)

by FREESCALE
Add-on patches to resolve issues in i.MX 6Quad and i.MX 6Dual Android GA BSP.
  • Date : 11/27/2012
  • Format : gz
  • Size : 8K
Download

IMX6_R13.4_GA.02_ANDROID_PATCH (REV 13.4-ga.02)

by FREESCALE
Patch release to support the new i.MX 6Qual/6Quad Rev C SABRE SDP and SDB boards with a stable DDR configuration and better camera preview quality,...
  • Date : 11/30/2012
  • Format : gz
  • Size : 403736K
https://www.freescale.com/webapp/Download?colCode=IMX6_R13.4_GA.02_ANDROID_PATCH&appType=license&loc...

IMX6_R13.5_01_ANDROID_PATCHES(REV R13.5-GA.01)

by FREESCALE
Android 13.5.0-GA.01 patch release. It adds camera support (USB and CSI camera), provides some bug fixes, and includes some regular updates. The.
Labels (3)
1 Reply

829 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi Don Freiling,

You do not need the above list of patches. The patch are for old version android BSP. The R13.4 is the version of android 4.0, this version need these patches to make board work fine. The version of L5.0.0 android BSP is the newest, it is based on the old version and do many improvement so you can use i

Have a great day,
Dan

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------