[Patches] (BSP 11.09.01 GA) camera/gstreamer/glib applications

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

[Patches] (BSP 11.09.01 GA) camera/gstreamer/glib applications

1,773 Views
RogerioNunes
NXP Employee
NXP Employee

Hi,

Working with a camera application recently I received the following two patches from factory that fix issues with glib (gprint) and gst-fsl-plugins (framerate):

Heard from EricNelson that more people had same issues, so it would be good to share.

There you go:

For glib:

---

dist/lfs-5.1/glib2/glib2.spec |    3 +++

1 file changed, 3 insertions(+)

diff --git a/dist/lfs-5.1/glib2/glib2.spec b/dist/lfs-5.1/glib2/glib2.spec

index dd9cbaf..6e77885 100644

--- a/dist/lfs-5.1/glib2/glib2.spec

+++ b/dist/lfs-5.1/glib2/glib2.spec

@@ -27,6 +27,9 @@ glib_cv_stack_grows=no \

glib_cv_uscore=no \

ac_cv_func_posix_getpwuid_r=yes \

ac_cv_func_posix_getgrgid_r=yes \

+glib_cv_long_long_format=ll \

+ac_cv_func_printf_unix98=yes \

+ac_cv_func_vsnprintf_c99=yes \

./configure --prefix=%{_prefix} --host=$CFGHOST --build=%{_build}

make

---


And for gst-fsl-plugins:

---

.../src/misc/v4l_source/src/mfw_gst_v4lsrc.c       |    4 ++--

1 file changed, 2 insertions(+), 2 deletions(-)

diff --git a/fsl_mm_linux/Multimedia/src/misc/v4l_source/src/mfw_gst_v4lsrc.c b/fsl_mm_linux/Multimedia/src/misc/v4l_source/src/mfw_gst_v4lsrc.c

index ec69d8f..4dbc645 100755

--- a/fsl_mm_linux/Multimedia/src/misc/v4l_source/src/mfw_gst_v4lsrc.c

+++ b/fsl_mm_linux/Multimedia/src/misc/v4l_source/src/mfw_gst_v4lsrc.c

@@ -513,8 +513,8 @@ mfw_gst_v4lsrc_capture_setup (MFWGstV4LSrc * v4l_src)

 

 

   parm.type = V4L2_BUF_TYPE_VIDEO_CAPTURE;

-  parm.parm.capture.timeperframe.numerator = v4l_src->fps_n;

-  parm.parm.capture.timeperframe.denominator = v4l_src->fps_d;

+  parm.parm.capture.timeperframe.numerator = v4l_src->fps_d;

+  parm.parm.capture.timeperframe.denominator = v4l_src->fps_n;

   parm.parm.capture.capturemode = v4l_src->capture_mode;

 

   input = v4l_src->input;

--

Labels (4)
0 Kudos
3 Replies

878 Views
tobiasschneider
Contributor I

Thanks for the patches, but could you also please give some explanation/reason for it? e.g. what the problems without have been in detail (e.g. with gprint?)

0 Kudos

878 Views
RogerioNunes
NXP Employee
NXP Employee

Without glib patch, g_print would crash, for instance, where a %p was used.

These patches are not necessary with the new BSP (L3.0.35_1.1.0_SOURCE), which I would suggest using instead.

0 Kudos

878 Views
EricNelson
Senior Contributor II

Thanks Rogerio!

0 Kudos