Hi,
We would like to use PF1510 for our implementation with IMX6ULL.
However, we noticed there is no driver available for this chip in Linux.
I found that the PF1550/PF1510 driver has been removed from the kernel:
https://community.nxp.com/t5/Power-Management/Linux-driver-for-PF1550-and-iMX6ULZ/td-p/1059763
I can only find pf1550-regulator-rpmsg.c in my kernel (im using NXP release 5.4.47_2.2.0 ).
I found in application note AN12922 that there is a patch available:
https://www.nxp.com/docs/en/application-note/AN12992.pdf
I was wondering where I would be able to find this patch, and if is different from the version in Linux NXP release 4.19.35_1.1.0 (pf1550.c) mentioned in the above post.
已解决! 转到解答。
Hi @r_veens ,
There's no existing patch about PF1510 enablement in i.MX6ULL. PF1510 driver can reuse the PF1550 driver. Cause PF1510 only removed charging function from PF1550.
You can refer to imx6ul-14x14-evk-pf1550.dts and pf1550.c file in former Linux BSP.
Hi @r_veens ,
There's no existing patch about PF1510 enablement in i.MX6ULL. PF1510 driver can reuse the PF1550 driver. Cause PF1510 only removed charging function from PF1550.
You can refer to imx6ul-14x14-evk-pf1550.dts and pf1550.c file in former Linux BSP.