Partition for eMMC before flashing imx6

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Partition for eMMC before flashing imx6

Jump to solution
1,893 Views
refiktuzaklı
Contributor III

I have problem with partition sizes. I dont know how to specify the partition size before flashing imx6-kara tx6 8033. I asked the question at stackexchange. Someone said it's about MFG Tool. But I don't know which configuration file does this partition. rootfs partition is just 300MB. it is not enough for my work

Can some one help how to control partition sizes before flashing imx6.

Labels (2)
Tags (2)
1 Solution
1,478 Views
refiktuzaklı
Contributor III

fdisk does not change rootfs size.

solution was just about ucl2.xml file. in line 104 under "LINUX_MMC" I have changed number 614400 after second "echo size" with 7700480. So now I can use rest of memory under third partition as second partition.

View solution in original post

2 Replies
1,479 Views
refiktuzaklı
Contributor III

fdisk does not change rootfs size.

solution was just about ucl2.xml file. in line 104 under "LINUX_MMC" I have changed number 614400 after second "echo size" with 7700480. So now I can use rest of memory under third partition as second partition.

1,478 Views
joanxie
NXP TechSupport
NXP TechSupport

one can refer to the enclosed document, pls focus on the chapter 4.3.3 Partitioning the SD/MMC card

0 Kudos
Reply