Parallel interface camera module for MCIMX6Q - SDB

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Parallel interface camera module for MCIMX6Q - SDB

2,397 次查看
sathyanarayanan
Contributor I

Hi 

   In MCIMX6Q - SDB evaulation kit to interface the camera module parallel interface(DVP) and MIPI is provided. Pls suggest the camera module which able to connect with MCIMX6Q - SDB Parallel(DVP) interface connector. 

Thanks in advance 

标签 (3)
0 项奖励
回复
4 回复数

1,866 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Sathyanarayanan

it is OV5642, p.8 spf-27392 Sabre schematic

Schematics (1)
i.MX6_SABRE_SDP_DESIGNFILES
http://www.nxp.com/products/software-and-tools/hardware-development-tools/sabre-development-system/s...

pastedImage_1.jpg

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

1,866 次查看
sathyanarayanan
Contributor I

Hi can you pls specify the exact part no of the module. pls note it should be mated with J9.

0 项奖励
回复

1,866 次查看
igorpadykov
NXP Employee
NXP Employee
0 项奖励
回复

1,866 次查看
mbogenschuetz
Contributor I

Does anyone know a matching replacement board for the above mentioned parallel camera OV05642-MRSL-A01A ?

The OV05642-MRSL-A01A is discontinued and cannot be bought anymore as far as I can see.

(see https://www.ovt.com/download/datasets/6355/2QF14%20PDN%20Notification%202013%200930.pdf )

0 项奖励
回复