Parallel camera I/F of i.MX7D

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Parallel camera I/F of i.MX7D

Jump to solution
922 Views
torus1000
Contributor V

Hi,

I plan to connect AR0134CS(1.2Mpix, mono, raw 12b) to the i.MX7D's parallel camera I/F.

According to the RM, i.MX7D support following data.

・8-bit/10-bit/16-bit/24-bit data port for generic data input.
・8-bit / 10-bit / 16-bit data port for Bayer data input.

How can I capture several still images?
Is it OK to configure 16b genric data input for mono 12b data capturing?

Can anyone help me?

Labels (2)
Tags (2)
0 Kudos
Reply
1 Solution
723 Views
weidong_sun
NXP TechSupport
NXP TechSupport

Hello torus,

   Although we don't have ready-made solution for your applicaiton, I think your connection is right.


Have a great day,
TIC  Weidong Sun

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
724 Views
weidong_sun
NXP TechSupport
NXP TechSupport

Hello torus,

   Although we don't have ready-made solution for your applicaiton, I think your connection is right.


Have a great day,
TIC  Weidong Sun

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply