Pad control register meaning for imx6q

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Pad control register meaning for imx6q

Jump to solution
1,429 Views
shuodo
Contributor II

In the "IOMUX controller" section (pinmux) of imx6q TRM, it has many pad control registers. I don't quite understand the meaning of some of the fields in these pad control registers:

15–14 Pull Up / Down Config. Field: e.g. 00 - 100K Ohm Pull Down, 01 - 47K Ohm Pull Up.

Does it mean that this pin can have internal resister pulled up/down? If it has internal resister pulled up, is it pulled up to 1.8V or 3.3V?

7–6 SPEED field: e.g. 01 - 100 MHz, if SRE=1: 100MHz @ 1.8V, 150MHz @ 3.3V

What does this speed field mean? And what determines whether it is at 1.8V or 3.3V?

5–3 Drive Strength Field: e.g. 011 - 50 Ohm @ 3.3V, 90 Ohm @ 1.8V

Again, What does this drive strength field mean? And what determines whether it is at 1.8V or 3.3V?

Labels (1)
Tags (1)
1 Solution
1,347 Views
igorpadykov
NXP Employee
NXP Employee

Hi Shuo

for pad control usage one can look at AN5078

Influence of Pin Setting on System Function and Performance

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

1 Reply
1,348 Views
igorpadykov
NXP Employee
NXP Employee

Hi Shuo

for pad control usage one can look at AN5078

Influence of Pin Setting on System Function and Performance

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------