Package Thermal Characteristics for i.MX27

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Package Thermal Characteristics for i.MX27

Jump to solution
969 Views
ko-hey
Senior Contributor II

Hi all

Does someone have thermal characteristics data for i.MX27 ?

I want a data which likes table 16 of IMX25AEC.pdf for calculation.

Ko-hey

Labels (1)
0 Kudos
Reply
1 Solution
818 Views
joanxie
NXP TechSupport
NXP TechSupport

yes, temperature in the datasheet is the ambient temperature

as Tj (junction temperature), R (thermal  resistance, that may be needed for thermal estimations are not provided.    Also thermal parameters are not specified, but they are taken  into account implicitly.  max Tj = max Ta + R * Pd,  where Tj - junction temperature ; Ta - ambient temperature from the datasheet ; R - thermal resistance ;  Pd - power dissipation in package.  For i.MX27 production technology  the junction temperature is ~105C.

View solution in original post

0 Kudos
Reply
4 Replies
818 Views
joanxie
NXP TechSupport
NXP TechSupport

I upload the 19X19 imx31 data, but this is the same as imx27.

0 Kudos
Reply
818 Views
ko-hey
Senior Contributor II

Hi Joan Xie

Let me confirm one more thing.

What is the junction temperature for i.MX27 ?

The datasheet shows only temperature like below.

So I can't clarify whether the temperature is junction temperature or not.

pastedImage_4.png

Furthermore, according to the following product selector, it shows ambient operating temperature.

pastedImage_3.png

As a result, the temperature which shows in table 1 of datasheet isn't junction temperature.

So please tell me the junction temperature for i.MX27.

Ko-hey

0 Kudos
Reply
818 Views
ko-hey
Senior Contributor II

Could someone follow and support this question ?

Ko-hey

0 Kudos
Reply
819 Views
joanxie
NXP TechSupport
NXP TechSupport

yes, temperature in the datasheet is the ambient temperature

as Tj (junction temperature), R (thermal  resistance, that may be needed for thermal estimations are not provided.    Also thermal parameters are not specified, but they are taken  into account implicitly.  max Tj = max Ta + R * Pd,  where Tj - junction temperature ; Ta - ambient temperature from the datasheet ; R - thermal resistance ;  Pd - power dissipation in package.  For i.MX27 production technology  the junction temperature is ~105C.

0 Kudos
Reply