PWR_CFG bit in PF3000 datasheet.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

PWR_CFG bit in PF3000 datasheet.

Jump to solution
618 Views
satoshishimoda
Senior Contributor I

Hi community,

I have a question about PF3000 datasheet.

Please see the description of RESTARTEN bit in Table 124 of the datasheet.

It mentions about PWR_CFG bit in this description, but I cannot find this bit in other place.

So I think PWR_CFG bit is typo and PWRON_CFG bit is correct, is this right?

Best Regards,

Satoshi Shimoda

Labels (1)
Tags (1)
0 Kudos
Reply
1 Solution
505 Views
igorpadykov
NXP Employee
NXP Employee

Hi Satoshi

right, PWR_CFG bit is typo and PWRON_CFG bit is correct.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
506 Views
igorpadykov
NXP Employee
NXP Employee

Hi Satoshi

right, PWR_CFG bit is typo and PWRON_CFG bit is correct.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply