PWM of IMX6SX cannot be generated continuously

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

PWM of IMX6SX cannot be generated continuously

Jump to solution
1,092 Views
longh
Contributor III

Hi All,

   I am working on

pwm changes randomly 

0 Kudos
Reply
1 Solution
1,066 Views
igorpadykov
NXP Employee
NXP Employee

Hi long

if PWM cannot be generated continuously one can check

if it is disabled in low power modes, bits DOZEN, STOPEN, WAITEN

described in sect.49.7.1 PWM Control Register (PWMx_PWMCR)

i.MX 6SoloX Applications Processor Reference Manual

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
1,067 Views
igorpadykov
NXP Employee
NXP Employee

Hi long

if PWM cannot be generated continuously one can check

if it is disabled in low power modes, bits DOZEN, STOPEN, WAITEN

described in sect.49.7.1 PWM Control Register (PWMx_PWMCR)

i.MX 6SoloX Applications Processor Reference Manual

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply