PSWITCH left unconnected and DCDC issue

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

PSWITCH left unconnected and DCDC issue

Jump to solution
2,515 Views
dgotfroi
Contributor IV

Hello all,

I use a IMX28 with an external +5V power supply. I don't have any battery connected.

So, can I leave PSWITCH unconnected or do I have to tie it to GND or other ?

Second question, since I don't use a battery, do I need to connect something to "Battery", "DCDC_BATT" and "VDD4P2" ?

I followed the schematic of the evaluation board and my shematic looks like that :

DCDC.JPG.jpg

But "VBAT" is leave unconnected, so can I remove C1 to C10, R1 to R4, D1 and L1 ?

Many thanks

Labels (1)
1 Solution
1,710 Views
victorien
Contributor IV
0 Kudos
Reply
4 Replies
1,711 Views
victorien
Contributor IV

You can find the best way to supply your board on this document http://cache.freescale.com/files/32bit/doc/app_note/AN4199.pdf?fasp=1&WT_TYPE=Application%20Notes&WT... chapter 4

0 Kudos
Reply
1,710 Views
dgotfroi
Contributor IV

Many thanks for this very useful answer.

And what about PSWITCH ?

0 Kudos
Reply
1,710 Views
victorien
Contributor IV

If you need the recovery boot, you need to keep the same schematic as Evaluation Board. But if you don't use recovery and always supply to VDD5V, I thinks the best connection is to tie it to GND

1,710 Views
dgotfroi
Contributor IV

Many thanks for all. I had my answer :smileyhappy:.

0 Kudos
Reply