PSWITCH left unconnected and DCDC issue

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

PSWITCH left unconnected and DCDC issue

ソリューションへジャンプ
3,005件の閲覧回数
dgotfroi
Contributor IV

Hello all,

I use a IMX28 with an external +5V power supply. I don't have any battery connected.

So, can I leave PSWITCH unconnected or do I have to tie it to GND or other ?

Second question, since I don't use a battery, do I need to connect something to "Battery", "DCDC_BATT" and "VDD4P2" ?

I followed the schematic of the evaluation board and my shematic looks like that :

DCDC.JPG.jpg

But "VBAT" is leave unconnected, so can I remove C1 to C10, R1 to R4, D1 and L1 ?

Many thanks

ラベル(1)
1 解決策
2,200件の閲覧回数
victorien
Contributor IV
0 件の賞賛
返信
4 返答(返信)
2,201件の閲覧回数
victorien
Contributor IV

You can find the best way to supply your board on this document http://cache.freescale.com/files/32bit/doc/app_note/AN4199.pdf?fasp=1&WT_TYPE=Application%20Notes&WT... chapter 4

0 件の賞賛
返信
2,200件の閲覧回数
dgotfroi
Contributor IV

Many thanks for this very useful answer.

And what about PSWITCH ?

0 件の賞賛
返信
2,200件の閲覧回数
victorien
Contributor IV

If you need the recovery boot, you need to keep the same schematic as Evaluation Board. But if you don't use recovery and always supply to VDD5V, I thinks the best connection is to tie it to GND

2,200件の閲覧回数
dgotfroi
Contributor IV

Many thanks for all. I had my answer :smileyhappy:.

0 件の賞賛
返信