PSWITCH left unconnected and DCDC issue

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

PSWITCH left unconnected and DCDC issue

跳至解决方案
2,908 次查看
dgotfroi
Contributor IV

Hello all,

I use a IMX28 with an external +5V power supply. I don't have any battery connected.

So, can I leave PSWITCH unconnected or do I have to tie it to GND or other ?

Second question, since I don't use a battery, do I need to connect something to "Battery", "DCDC_BATT" and "VDD4P2" ?

I followed the schematic of the evaluation board and my shematic looks like that :

DCDC.JPG.jpg

But "VBAT" is leave unconnected, so can I remove C1 to C10, R1 to R4, D1 and L1 ?

Many thanks

标签 (1)
1 解答
2,103 次查看
victorien
Contributor IV
0 项奖励
回复
4 回复数
2,104 次查看
victorien
Contributor IV

You can find the best way to supply your board on this document http://cache.freescale.com/files/32bit/doc/app_note/AN4199.pdf?fasp=1&WT_TYPE=Application%20Notes&WT... chapter 4

0 项奖励
回复
2,103 次查看
dgotfroi
Contributor IV

Many thanks for this very useful answer.

And what about PSWITCH ?

0 项奖励
回复
2,103 次查看
victorien
Contributor IV

If you need the recovery boot, you need to keep the same schematic as Evaluation Board. But if you don't use recovery and always supply to VDD5V, I thinks the best connection is to tie it to GND

2,103 次查看
dgotfroi
Contributor IV

Many thanks for all. I had my answer :smileyhappy:.

0 项奖励
回复