Hi!
Following code is copied from my imx33 pin_mux.dts
Can it be a clock problem?
/ {
model = "NXP i.MX 93 Based Custom Board";
compatible = "fsl,imx93-custom-board", "fsl,imx93";
soc {
#address-cells = <1>;
#size-cells = <1>;
iomuxc: iomuxc@443C0000 {
compatible = "fsl,imx93-iomuxc";
reg = <0x443C0000 0x470>;
};
};
};
&iomuxc {
pinctrl-names = "default_iomuxc";
pinctrl-0 = <&BOARD_InitPins>;
imx93-custom-board {
BOARD_InitPins: BOARD_InitPinsgrp { /*!< Function assigned for the core: Cortex-M33[cm33] */
/*
* TEXT BELOW IS USED AS SETTING FOR TOOLS *************************************
BOARD_InitPins:
- options: {callFromInitBoot: 'true', coreID: cm33}
- pin_list:
- {pin_num: L18, peripheral: LPUART6, signal: lpuart_rx, pin_signal: GPIO_IO05}
- {pin_num: L17, peripheral: LPUART6, signal: lpuart_tx, pin_signal: GPIO_IO04}
* BE CAREFUL MODIFYING THIS COMMENT - IT IS YAML SETTINGS FOR TOOLS ***********
*/
fsl,pins = <
MX93_PAD_GPIO_IO04__LPUART6_TX 0x0000051E
MX93_PAD_GPIO_IO05__LPUART6_RX 0x0000051E
>;
};
};
};