PORTING ANDROID TO i.MX23evk

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

PORTING ANDROID TO i.MX23evk

Jump to solution
1,477 Views
shanmugamsundar
Contributor IV

hi all,

        I am new to i.MX23 evk, i want to port the android on the evk, is it possible to port it?, can any one help me, if its so plz share me how to get the linux android BSP for i.MX23evk,

Thanks,

shan

Labels (4)
0 Kudos
1 Solution
1,019 Views
MT
NXP Employee
NXP Employee
0 Kudos
4 Replies
1,020 Views
MT
NXP Employee
NXP Employee

I believe that Allgo Embedded a Freescale Partner did an Android port.

http://www.freescale.com/webapp/dap.detail.framework?CUSTOMER=ALEMR&company=ALLGO%2BEMBEDDED%2BSYSTE...

0 Kudos
1,020 Views
hippo
NXP TechSupport
NXP TechSupport

Freescale has no Android port for the i.MX233 processor and no plans to make it. The main reason is that this processor seems to have not enough performance to provide convenient operation of Android OS on it. The main Android-targeted members of the i.MX processors family are now i.MX51, i.MX53, and i,MX6.

Please look at link below for supported BSPs (Linux, WinCE)

http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=IMX23_SW

1,019 Views
shanmugamsundar
Contributor IV

hi hippo,

    i had downloaded the Linux kernel source for i.MX233, in that i need to port QT GUI application, can you help me on how to port the QT and cross compiling the source.

Thanks,

shan

0 Kudos
1,019 Views
Yuri
NXP Employee
NXP Employee

The following may be helpful :

All Boards Qt v2

0 Kudos