POR signal and Power-up sequence for i.MX6

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

POR signal and Power-up sequence for i.MX6

1,326 Views
yuuki
Senior Contributor II

Dear all,

We want to use POR signal to reset i.MX6 during system working.
Is the POR signal able to be asserted while all power supplies to i.MX6 are stable?

Does i.MX6 need Power up sequence when POR signal is asserted?

Best Regards,
Yuuki

Labels (1)
Tags (2)
0 Kudos
Reply
1 Reply

1,063 Views
igorpadykov
NXP Employee
NXP Employee

Hi Yuuki

yes power up sequence should be followed when POR signal is asserted.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply