PF3000 vs PF3001 on i.mx6 ULL
Our board is very similar to the evaluation board:
https://community.nxp.com/docs/DOC-339884
but we have the ULL processor instead of the UL.
I can't undestand the difference beetwen PF3000 and PF3001.
In PF3001 page
there is the MCU compatibility list
In PF3000 page
the list is:
Inside neither datascheet there is a reference to ull series.
Whitch is the best PMIC for ULL processor?
Thank you
Elisa
Hello,
PF3000 and 3001 are pin to pin compatible.
PF3001 is a subset of PF3000.
PF3000 address Low Power application and target i.MX 7S/D, i.MX 6SL, i.MX 6SX
PF3001 address Always ON application and specially target Low end application, based on i.MX 6UL
PF3000 can be considered first for Low Power apps.
For simple application the PF3001 as most economical alternative can be selected.
I expect for Your i.MX 6ULL the PF3001 is a reasonable choice.
Have a great day,
Yuri
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.