PMIC SWBSTFB Max Rating

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

PMIC SWBSTFB Max Rating

跳至解决方案
1,358 次查看
danielkubiak
Contributor I

Hello,

The SWBSTFB max rating voltage is only 4.8V in the PF0100 data sheet (page 9).

It's a little bit surprising as the boost output voltage can go up to 5,15V.

标签 (1)
0 项奖励
回复
1 解答
1,254 次查看
JorgeRama_rezRi
NXP Employee
NXP Employee

Hi Daniel,

This error has already been detected. The correct value is 5.5V. This is being corrected in the next rev of the datasheet, which should be released in the next couple of weeks.

Best regards.

Jorge.

在原帖中查看解决方案

0 项奖励
回复
2 回复数
1,255 次查看
JorgeRama_rezRi
NXP Employee
NXP Employee

Hi Daniel,

This error has already been detected. The correct value is 5.5V. This is being corrected in the next rev of the datasheet, which should be released in the next couple of weeks.

Best regards.

Jorge.

0 项奖励
回复
1,254 次查看
danielkubiak
Contributor I

Hi Jorge,

Thank you for your answer.

Best Regards

Daniel

0 项奖励
回复