PMIC POR_B Delay

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

PMIC POR_B Delay

1,994 Views
katrinagundal-z
Contributor I

How long after the PMIC POR_B is released from low to high does it take to read the config bits? Since we use a mux (FET switch) on these lines which are also used as the EIM interface to the FPGA we need to ensure we hold the enable signal to this low long enough.

I tried tying POR_B directly to the mux so it releases on the same edge as the i.MX6. (It says somewhere that these are sampled on the edge of por_B rising. It won’t boot in this case. This mux enable needs to be delayed for some amount of time and I need to know how long that is..

Labels (2)
Tags (1)
0 Kudos
Reply
1 Reply

1,829 Views
igorpadykov
NXP Employee
NXP Employee

Hi Katrina

one can use solution used in i.MX6SL EVK, spf-27452   p.13

iMX6SL_EVK_DESIGNFILES  : Design files, including hardware schematics

spf-27452   p.13.jpg

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply