PMIC_ON_REQ design on i.MX7 SABRE.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

PMIC_ON_REQ design on i.MX7 SABRE.

Jump to solution
1,428 Views
satoshishimoda
Senior Contributor I

Hi community,

Our customer have a question about i.MX7 SABRE board.
Please see the following image, it shows the connection of PMIC_ON_REQ signal.

IMG_0298.JPG


PMIC_ON_REQ is push-pull output from Table 8 in IMX7DSHDG Rev.0, and RESET_B of reset IC is open-drain from TPS3808 datasheet.
If i.MX7 output PMIC_ON_REQ as High and reset IC output output RESET_B as low at the same time, we think output collision will be occurred and short will be also occurred as the red route on the following image.

IMG_0298_2.jpg
So pull-down resistor should be added between PMCI_ON_REQ and RESET_B (at the black square).
Is our understanding correct?
Or the SABRE shematic is no problem with some reason?


Best Regards,
Satoshi Shimoda

Labels (2)
Tags (1)
0 Kudos
1 Solution
927 Views
art
NXP Employee
NXP Employee

Yes, you are right. R307 should be either not populated or be at least some 1 to 10 kOhm resistor to prevent extra current drain when the external watchdog Reset signal goes Low.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
2 Replies
928 Views
art
NXP Employee
NXP Employee

Yes, you are right. R307 should be either not populated or be at least some 1 to 10 kOhm resistor to prevent extra current drain when the external watchdog Reset signal goes Low.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
927 Views
satoshishimoda
Senior Contributor I

Hi Artur,

OK, we understood.

And please tell this problem to your SABRE development team to fix this problem on next revision.

Best Regards,

Satoshi Shimoda

0 Kudos