PMIC GUI: Program and Verify Buttons not highlighted

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

PMIC GUI: Program and Verify Buttons not highlighted

2,627件の閲覧回数
michaelbazarov
Contributor II


Hello all,

I am using GUI Rev 4 and the PMIC PF0100 Eval board along with the socket board to try and set OTP fuses on unprogrammed PMICs. I have the script for the configuration I want but the program and verify buttons are not clickable. I placed J17 jumpers accross pins 1 and 2 to allow OTP programming and ran my OTP script in the script editor. Pretty sure I burned the fuses on the embedded eval board PMIC but when I click "Blank device" it now says device programmed when before it said device blank. Is there a way to get the GUI to verify my configuration? Did i even program the new part i placed in the socket board or just the one on the eval board?

Thanks,

Mike

0 件の賞賛
返信
5 返答(返信)

2,485件の閲覧回数
art
NXP Employee
NXP Employee

Please refer to the Chapter 5 of the attached document.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

2,485件の閲覧回数
weidong_sun
NXP TechSupport
NXP TechSupport

Hi Mike,

   It the part has already programmed, when the board connect to the GUI, Enable Target, the “Buck Supplies” and “Linear Supplies”  panel will show the fuses information about the part, you can check if this is what you want.

To do the program, after load the script, it needs to click the “Convert Script File” button on the bottom firstly, then you will the the “PROGRAM”  button will switch from gray to green. It is recommended to click “Verify After Programming” button at the same time.

Reards,

Weidong

0 件の賞賛
返信

2,485件の閲覧回数
michaelbazarov
Contributor II

"To do the program, after load the script, it needs to click the “Convert Script File” button on the bottom firstly, then you will the the “PROGRAM”  button will switch from gray to green. It is recommended to click “Verify After Programming” button at the same time."

I did that and the Program button never turned green.

Are the Buck and Linear Supplies Panels showing configuration for both the PMIC soldered to the EVAL board AND the loose PMIC part I placed into the socket programmer board that is plugged into the EVAL board I2c header?

Thanks,

Mike

0 件の賞賛
返信

2,485件の閲覧回数
art
NXP Employee
NXP Employee

What socket programmer board do you use? Please specify.

Have a great day,

Artur

0 件の賞賛
返信

2,485件の閲覧回数
michaelbazarov
Contributor II

KITPF0100SKTEVBE

700-27867 Rev B

SCH-27867 Rev B

Thanks,

Mike

0 件の賞賛
返信