Hi,
I am using PF3001 with iMX6UL in one of my design.
I am facing issue with PF3001. I am using 5V adapter to powerup the board. As recommended in PF3001, I have used external P-MOSFET.
Prior to this issue, PMIC power was ok and I was able to boot iMX6UL.
Now MOSFET is not turning ON. I have observed that Gate (LDOG) voltage and Source voltage (VPWR) are same, 5V.
From below image (PF3001 datasheet Page # 31) it seems that it is only possible when internal PNP transistor is off.
Is there any damage internally in PF3001?
Thanks,
Ritesh
Any though/solution on above ..???
Seeking for earliest response.....