PF3000 : unused pin treatment

cancel
Showing results for 
Search instead for 
Did you mean: 

PF3000 : unused pin treatment

Jump to solution
386 Views
koichisakagami
Contributor II

Dear community,
We have been developing our product with PF3000.
I have a question about  PF3000 unused pin treatment.

In Data sheet PF3000 Rev. 7.0, Table 2. Pin definitions (Notes 3),
it is described that the Unused switching regulators treatment.
    Pins SWxLX and SWxFB should be unconnected and Pin SWxIN should be
    connected to VIN with a 0.1 μF bypass capacitor.

But the unused LDO Linear regulators treatment is not described.

[Question]
       Could you teach me the unused LDO Linear regulators pins handling ?

Best Regards,
    Koichi Sakagami

Labels (1)
0 Kudos
1 Solution
185 Views
Yuri
NXP TechSupport
NXP TechSupport

Hello,

  LDO outputs may be left floating, input voltage must be provided.

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
3 Replies
186 Views
Yuri
NXP TechSupport
NXP TechSupport

Hello,

  LDO outputs may be left floating, input voltage must be provided.

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
185 Views
kanoumamoru
Contributor III

Hi Yuri,

I have One more question in this topic.

Why  LDO input voltage is necessary ?

We intend to pull down unused LDO input pin to GND.

That is, LDO input voltage = 0V.

Is it OK in this case ?

Kanou

0 Kudos
185 Views
Yuri
NXP TechSupport
NXP TechSupport

Hello,

  All PMICs of PF series require all supply inputs powered, at least,

in order to avoid leakages. 

Regards,

Yuri.

0 Kudos