PF3000 stand by power scaling

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

PF3000 stand by power scaling

1,264件の閲覧回数
analogicstechin
Contributor III

 Here we using PF3000 power management IC ,IMX6ULL SOC.

About our custom device  enter into standby mode (i.e echo  mem > /sys/power/state )   PMIC_STBY_REQ  pin(ball U9) become high ,but  we observed  any change in the output  voltage changes of PF3000 (like VDD_ARM_SOC_IN ) .please suggest related driver implementation or any suggestion.

NOTE : The same pin is connected to  PF3000 standby pin.

ラベル(7)
2 返答(返信)

1,138件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Analogics

these settings are defined in uboot, please check for example mx6ull_ddr3_arm2.c,

function power_init_board()

uboot-imx.git - Freescale i.MX u-boot Tree 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

1,138件の閲覧回数
analogicstechin
Contributor III

Thank you igorpadykov ,

very useful information .

0 件の賞賛
返信