PF3000 : VCC_SD voltage transition time

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

PF3000 : VCC_SD voltage transition time

ソリューションへジャンプ
1,192件の閲覧回数
koichisakagami
Contributor II

Dear community,
We have been developing our product with PF3000.
I have a question about  VCC_SD voltage transition time.

The VCC_SD voltage is switched by SD_VSEL logic level.

[Question]
       How long time does it take to switch the VCC_SD voltage range by changing SD_VSEL ?

    Best Regards,
    Koichi Sakagami

ラベル(1)
0 件の賞賛
返信
1 解決策
1,103件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Koichi

unfortunately this time is not specified by datasheet, however one

can estimate it using formula : I*t=C*U,

I=100mA, U=3V (SD_VSEL, Vh-Vl),C=2.2uF,

t~60uS

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,104件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Koichi

unfortunately this time is not specified by datasheet, however one

can estimate it using formula : I*t=C*U,

I=100mA, U=3V (SD_VSEL, Vh-Vl),C=2.2uF,

t~60uS

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信