PF3000 : Start-up timing diagram

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

PF3000 : Start-up timing diagram

Jump to solution
1,362 Views
koichisakagami
Contributor II

Dear community,
We have been developing our product with PF3000.
I have a question about  Start-up timing diagram.

In Data sheet PF3000 Rev. 7.0, 6.3.3.1 Start-up timing diagram,
it is described that the Start-up timing diagram begins at (VSNVS = 0v) point.

I would like to know the Start-up timing diagram which begins at (VSNVS from LICELL) point.
In the case of MMPF0100, VSNVS starts from 1.0V if LICELL is valid before VIN.

[Question]

Is PF3000 the same behavior as MMPF0100 ?

       Best Regards,
       Koichi Sakagami

Labels (1)
0 Kudos
Reply
1 Solution
1,231 Views
art
NXP Employee
NXP Employee

Q. Is PF3000 the same behavior as MMPF0100 ?

A. Yes, the VSNVS output of the PF3000 PMIC behaves the same way as of the PF0100 one.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
2 Replies
1,231 Views
koichisakagami
Contributor II

Dear Artur san,

Thank you for your reply.

I got it.

Best Regards,

Koichi Sakagami

0 Kudos
Reply
1,232 Views
art
NXP Employee
NXP Employee

Q. Is PF3000 the same behavior as MMPF0100 ?

A. Yes, the VSNVS output of the PF3000 PMIC behaves the same way as of the PF0100 one.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply