PF3000 : SNVS,SW-Reg overcurrent behavior

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

PF3000 : SNVS,SW-Reg overcurrent behavior

Jump to solution
1,871 Views
kanoumamoru
Contributor III

Hi, community.

PF3000 has some LDOs and SW-Regs.

Each regulators have over current detector or limiter. 

But we can't find the description about Current limit protection behavior
for SNVS and SW regulator in the data sheet.

Q1) Are there current limiter for SNVS ?

Q2) Are there current limiter for switching regulator (i.e. SW1A/1B, SW2, SW3) ?

Best Regards,

kanou

Labels (2)
1 Solution
1,674 Views
RossMcLuckie
NXP Employee
NXP Employee

Hi Kanou,

The SNVS LDO is only capable of 1mA maximum, so current limiting doesn't make much sense at those levels, it is also intended as an always on supply, so if something goes wrong there your whole system is likely to fail, should only be connected to the iMX etc, so the likelihood of failing should be minimal.

The SW's do have current limiting and can generate interrupts if tripped, see the control registers in the datasheet -

pastedImage_1.png

pastedImage_2.png

Regards

Ross

View solution in original post

2 Replies
1,674 Views
art
NXP Employee
NXP Employee

1. The SNVS LDO doesn't have the current limiting function since this is very low-power LDO primarily meant to backup the RTC and SNVS logic of a processor in power-off mode.

2. The switching regulators have the current limiting function, refer to the part's documentation.


Have a great day,
Artur

0 Kudos
Reply
1,675 Views
RossMcLuckie
NXP Employee
NXP Employee

Hi Kanou,

The SNVS LDO is only capable of 1mA maximum, so current limiting doesn't make much sense at those levels, it is also intended as an always on supply, so if something goes wrong there your whole system is likely to fail, should only be connected to the iMX etc, so the likelihood of failing should be minimal.

The SW's do have current limiting and can generate interrupts if tripped, see the control registers in the datasheet -

pastedImage_1.png

pastedImage_2.png

Regards

Ross