PF3000/01 + i.MX 6SoloX

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

PF3000/01 + i.MX 6SoloX

757件の閲覧回数
andy_kim
Contributor IV

Hello,

The PF0200 is the referenced-PMIC on the i.MX 6 SoloX SABRE board.

When I check i.MX & PMIC Match table,

It seems that a patch for i.MX 6 SoloX is needed to apply PF3000/01 to it.

What I would like to know how to patch for it and which document do I need to refer to for that?

 

Thanks,

Andy

0 件の賞賛
返信
1 返信

739件の閲覧回数
AldoG
NXP TechSupport
NXP TechSupport

Hello,

Driver for PF100, PF200 and PF3000 is the same so the only changes that you may need are in dts for uboot and Linux/Android, for this purpose you can take as reference dts from another board such as:

https://source.codeaurora.org/external/imx/uboot-imx/tree/arch/arm/dts/imx7d-sdb.dts?h=imx_v2020.04_...

https://source.codeaurora.org/external/imx/linux-imx/tree/arch/arm/boot/dts/imx7d-sdb.dts?h=imx_4.14...

Here you'll see PF3000 is connected to I2C1. This will depend on how you connected the PMIC in your design. So, you can take this as an example and add the code in your board dts file.

Best regards,
Aldo.

0 件の賞賛
返信