PF1550+i.MX6ULL recommended connection for INT2P7

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

PF1550+i.MX6ULL recommended connection for INT2P7

874件の閲覧回数
yuji_matsunami
Contributor II

Hi,
Regarding application note(AN12055)
The application note(AN12055) has been updated Rev2.0 and the connections of 38pin(INT2P7) have changed when not used.
What is the reason for the change?
also, what will happen if 38pin(INT2P7) is floating ?


AN12055 Rev2.0    Page.2
38pin INT2P7 Recommended connection when not used : Bypass with 2.2uF capacitor to ground

AN12055 Rev1.0     Page.3
38pin INT2P7 Recommended connection when not used : Leave floating

0 件の賞賛
返信
1 返信

863件の閲覧回数
jamesbone
NXP TechSupport
NXP TechSupport

The change it is only for a better termination of the PIN, for removing the power distortion and noise and protect the system/IC by providing pure DC supply.

 

0 件の賞賛
返信