PF1510 PMIC I2C_ADDR register 0x68

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

PF1510 PMIC I2C_ADDR register 0x68

ソリューションへジャンプ
2,231件の閲覧回数
Migli0
Contributor III

Hello,

what is the purpose of the USE_DEFAULT_ADDR bit (7) of this register?

marcomigliore_0-1660293718305.png

I did not find any details on the datasheet.

My assumption is that is if current I2C address is different from the default, setting that bit will switch to the default I2C address (0x08). Is that correct?

What will happen then if the current I2C address is already 0x08? Will setting that bit be completely harmless?

 

Best Regards,

Marco

0 件の賞賛
返信
1 解決策
2,178件の閲覧回数
diazmarin09
NXP TechSupport
NXP TechSupport

Hello Marco,

Thank you for using the NXP communities. It is our pleasure.

You are correct, the I2C address of PF1510 cannot be changed and it is fixed for a specific part number.

So, setting this bit will have no effect on the device behavior.

Regards,

David

元の投稿で解決策を見る

3 返答(返信)
2,187件の閲覧回数
diazmarin09
NXP TechSupport
NXP TechSupport

Hello Marco,

I hope all is great with you.

In this case, please  consider the I2C device address as 0x08.

Unfortunately, the I2C address of PF1510 cannot be changed and it is fixed for a specific part number.

I hope this information helps.

Regards,

David

0 件の賞賛
返信
2,182件の閲覧回数
Migli0
Contributor III

Hello David,

thanks for the reply.

I don't actually need to change the default I2C address, 0x08 is fine for us.

So based on your statement, that the address is fixed, can you please confirm me that setting/clearing USE_DEFAULT_ADDR bit (7), in register 0x68, will be completely harmless, and it will not harm PMIC behaviour at all?

 

Many thanks,

Marco

0 件の賞賛
返信
2,179件の閲覧回数
diazmarin09
NXP TechSupport
NXP TechSupport

Hello Marco,

Thank you for using the NXP communities. It is our pleasure.

You are correct, the I2C address of PF1510 cannot be changed and it is fixed for a specific part number.

So, setting this bit will have no effect on the device behavior.

Regards,

David