PF0100 coin cell charger current

cancel
Showing results for 
Search instead for 
Did you mean: 

PF0100 coin cell charger current

360 Views
emil
Contributor III

Hello,

I see in the datasheet to the PF0100 that the coin cell charger current only is 60uA. Can this be correct? That would mean that it would take 750 hours to fully charge a 45mAh coin cell battery. And at at discharge rate of 10uA I would have to keep the device on four hours a day.

Please advice.

BR,

Emil Käll

Labels (1)
Tags (1)
0 Kudos
1 Reply

174 Views
igorpadykov
NXP TechSupport
NXP TechSupport

Hi emil

document is correct, for coin cell charging one

can use external charger as well.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos