PF0100 PMIC in the SCM-i.MXD/Q settings

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

PF0100 PMIC in the SCM-i.MXD/Q settings

1,201 Views
RussellPead
Contributor II

1)     Is the PF0100 PMIC in the SCM-i.MX6D/Q preprogrammed?

2)     If so, what are the settings?

Russell

Labels (3)
Tags (3)
0 Kudos
Reply
2 Replies

920 Views
amanda_mcgregor
NXP Employee
NXP Employee

Hi Russell,

Additional information from our hardware designer, see below.

Yes we will program the PF100 but also leave the fuses open for customers to burn the LDO values.

As we discovered with the camera, the power needs to be hardware driven, not SW enabled.

Otherwise the customer will require a board level LDO for the power critical timing circuits.

Cheers,

Amanda

0 Kudos
Reply

920 Views
art
NXP Employee
NXP Employee

For the detailed information on the integrated MMPF0100 power supply of the SCM-i.MX6D/Q Single Chip Module product, please refer to the Chapter 5 of its Data Sheet document, available on the product's Documentation web page:

http://www.nxp.com/products/single-chip-modules/single-chip-module-i.mx-6q:SCM-i.MX6Q?fpsp=1&tab=Doc...


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply