PF0100 Default configuration

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

PF0100 Default configuration

ソリューションへジャンプ
1,293件の閲覧回数
abhijit_mote
Contributor I

1. In default mode of PF0100 there is no mention about the following supplies:

SWBST_VOLT, VGEN1_VOLT and VGEN3_VOLT. Does it mean that these supplies are not enabled?

2. Default configuration of register SWBSTCTL as per data sheet says the SWBST_VOLT is configured as 'ON' and configured for 5.0V.

3. For LDO's there are 4 bits (3:0) for output setting marked as VGENx (Register VGENxCTL) and its default value is mentioned as 0x80. The maximum value 4 bits can achieve is 0x0F. Is this a typing mistake? 

Refer the attachment below for more details.

タグ(1)
0 件の賞賛
返信
1 解決策
1,053件の閲覧回数
art
NXP Employee
NXP Employee

1. The SWBST, VGEN1 and VGEN3 supplies are by default Off in the Default power-on configuration.

2. There is no single reset configuration for supply control registers, it depends on the power-on configuration selected.

3. This is just a typo. Of course, the value of 0x8 is meant.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,054件の閲覧回数
art
NXP Employee
NXP Employee

1. The SWBST, VGEN1 and VGEN3 supplies are by default Off in the Default power-on configuration.

2. There is no single reset configuration for supply control registers, it depends on the power-on configuration selected.

3. This is just a typo. Of course, the value of 0x8 is meant.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信