PCM to I2S format conversion

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

PCM to I2S format conversion

5,922件の閲覧回数
jamesdeepu
Contributor II

I have two bluetooth chips connected to IMX6 via I2s interfaces. BT chip1 currently supports PCM format audio data and BT Chips2 supports audio in I2S format.

How will I convert PCM format audio data from BT chip1 to I2S format for BT Chip2 ?

thanks in advance.

ラベル(2)
0 件の賞賛
返信
2 返答(返信)

3,954件の閲覧回数
guslabao
Contributor III

HI Igor,

Can the SSI interface on IMX6 support the following PCM formats below?  What mode should the SSI be in to support either the long  or short frame sync? 

Thanks Gus.pastedImage_0.png

0 件の賞賛
返信

3,954件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi James

PCM is generic abbreviation used for many kinds of formats

Pulse-code modulation - Wikipedia, the free encyclopedia

you can analyze what is used by BT1 from its datasheet and

check if this could be supported by i.MX6 audio modules: SSI or ESAI,

then configure audio driver appropriately. Please check Chapter 25,61

i.MX6DQ Reference Manual (rev.2  7/2014)

http://cache.freescale.com/files/32bit/doc/ref_manual/IMX6DQRM.pdf

Processor can not convert one PCM format to another.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信