PCIe to USB reset in iMX6

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

PCIe to USB reset in iMX6

665 Views
balashanmugam
Contributor III

Hi Support Team,

Please find our configuration

1) Only we have problem with USB ports.

a) At USB2.0 connectors when we do mass storage transfer, we are facing the issue it is failing to write on the storage device.

b) At Bluetooth device (through Mini PCIe connector), when we do data transfer, sometimes it is crashing.

c) At LTE controller, Once the signal lost,  not establishing the network connection again

2) The Other PCIe devices connected to the PCIe switch PI7C9X2G404SL

1) WIFI module (through Mini PCIe) is working fine.

2) PCIe to ethernet controller is working fine.

Regards

Arulpandiyan Vadivel

Labels (4)
Tags (3)
0 Kudos
1 Reply

441 Views
igorpadykov
NXP Employee
NXP Employee

Hi Arulpandiyan

in general one can check nonworking peripherals connecting

them to i.MX6 PCIe port directly, without PI7C9X2G404SL switch.

If this will work, then seems problem in switch customization,

probably one can ask support from switch vendor.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos