PCIe on i.MX6 Duallite to FPGA

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

PCIe on i.MX6 Duallite to FPGA

5,032 Views
kerose
Contributor I

I need to perform a rapid prototype project for my company which runs off an i.MX6 Duallite processor running under Linux and communicating with an FPGA.  I am flexible on the FPGA at this time - but we will be using the FPGA for high speed measurements on 4 channels.

I would prefer to use an i.MX6 development board and some kind of FPGA development board so that I can begin to conduct a proof of concept.  I don't need 4 ADC channels at this time - the target data rate is 40 megasamples per second.  I will be using a FIFO core on the FPGA - I just want to demonstrate data retrieval in as near real-time as possible on the i.MX6 (and while I will be using an i.MX6 Duallite processor, I am also open to various i.MX6 processors for the sake of this demo).

My first goal is to connect the i.MX6 to the FPGA.  For the record, we are using a Xilinx Spartan 6 on an existing product, but I realize that may not be robust enough for a PCIe core.  I am open to an Altera FPGA as well.

0 Kudos
Reply
6 Replies

4,379 Views
igorpadykov
NXP Employee
NXP Employee

Hi Kevin

there are no restrictions on fpga and as starting point one can check links

https://community.freescale.com/docs/DOC-95014 

https://community.nxp.com/message/624345

Also may be useful to look at Chapter 40 PCI Express Root Complex Driver

attached Linux Manual.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

4,379 Views
kerose
Contributor I

Unfortunately, the links you give me do not provide much information - is there not a ready-made solution using the PCIe bus in some demo kit/development board?  I see information scattered at different places on the internet, but nothing concrete in how to use this bus.  I don't have time to fiddle with this.  Somebody somewhere knows how to do this.

0 Kudos
Reply

4,379 Views
igorpadykov
NXP Employee
NXP Employee

Hi Kevin

unfortunately there are no additional app notes or ready-made solutions

for fpga, sorry. Note,  NXP has Professional Services for helping to port custom drivers:

http://www.nxp.com/support/nxp-professional-services:PROFESSIONAL-SERVICE

Best regards
igor

0 Kudos
Reply

4,379 Views
kerose
Contributor I

So you are saying that engineers generally don't use the PCIe bus on the i.MX6?  If it is not useful as a port, then why does it exist?  I thought NXP would certainly have a reference design.  Since support does not exist for the PCIe bus on i.MX6, I will have to find another way to perform high speed communications.

0 Kudos
Reply

4,379 Views
igorpadykov
NXP Employee
NXP Employee

Hi Kevin

it was used, but not with fpga, please refer to sect.40.4.2 Tests

attached Linux Manual for tested devices.

Best regards
igor

0 Kudos
Reply

4,379 Views
kerose
Contributor I

Thank you! I will look into that.

Best regards

Kevin Rose

AA-AS/EDT4.1-NA

Tel. +1 805 880-9181

0 Kudos
Reply