PCIe of i.MX6 don’t work with external clock

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

PCIe of i.MX6 don’t work with external clock

Jump to solution
3,622 Views
massohy
Contributor II

Dear Community Member,

 

I am trying PCIe with new original board. Its PCIe is driven by external clock.  

PCIe use input clock from CLK_1N/P. Its clock is 100MHz and LVDS level.

 

I modified clk-imx6.c, pci-imx6.c and dts file in tune with inputting external clock in reference to this thread. i.MX6q PCIe with external clock and SATA https://community.nxp.com/thread/455537

 

    clocks {

        anaclk1 {

                compatible = "fixed-clock";

                reg = <0>;

                #clock-cells = <0>;

                clock-frequency = <100000000>;  /* 100MHz */

            };

    };

 

&pcie {

    status = "okay";

    clocks = <&clks IMX6QDL_CLK_PCIE_AXI>,

             <&clks IMX6QDL_CLK_LVDS1_IN>,

             <&clks IMX6QDL_CLK_PCIE_REF_125M>,

             <&clks IMX6QDL_PLL6_BYPASS>,

             <&clks IMX6QDL_PLL6_BYPASS_SRC>;

 

    clock-names = "pcie", "pcie_bus", "pcie_phy", "pcie_ext", "pcie_ext_src";

    ext_osc = <1>;

};

 

&clks {

        assigned-clocks = <&clks IMX6QDL_PLL6_BYPASS_SRC>,

                          <&clks IMX6QDL_PLL6_BYPASS>;

        assigned-clock-parents = <&clks IMX6QDL_CLK_LVDS1_IN>,

                                 <&clks IMX6QDL_PLL6_BYPASS_SRC>;

        assigned-clock-rates = <100000000>, <100000000>;

};

 

And I added this line in *.cfg file of u-boot in reference to this thread. Setting the iMX6 PCIe Clocks  https://community.nxp.com/docs/DOC-101788

DATA 4, 0x020c80e4, 0x00010501

 

But I encountered these messages at booting kernel.

 

1ffc000.pcie supply pcie-bus not found, using dummy regulator

imx6q-pcie 1ffc000.pcie: phy link never came up

imx6q-pcie 1ffc000.pcie: Failed to bring link up!

imx6q-pcie 1ffc000.pcie: failed to initialize host

imx6q-pcie: probe of 1ffc000.pcie failed with error -22

 

Please tell me where I should check and modify.

Labels (2)
0 Kudos
Reply
1 Solution
3,042 Views
igorpadykov
NXP Employee
NXP Employee

Hi mas

seems you are right, if external clock is used, pll is not needed.

You can try to test several pcie cards for "link-up" issue, recommended to use linux

from nxp repository

linux-imx - i.MX Linux kernel 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
4 Replies
3,042 Views
massohy
Contributor II

After I changed device tree like above, then CCM_ANALOG_PLL_ENET become to 0x00017000. It means PLL is down. Is it no problem because PCIe use external clock? Or should it be PLL locked and ENABLE_100M asserted?

0 Kudos
Reply
3,043 Views
igorpadykov
NXP Employee
NXP Employee

Hi mas

seems you are right, if external clock is used, pll is not needed.

You can try to test several pcie cards for "link-up" issue, recommended to use linux

from nxp repository

linux-imx - i.MX Linux kernel 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply
3,042 Views
massohy
Contributor II

Hi igor,

 

I succeeded to establish PCIe connection between i.MX6 and FPGA.

I replaced pci-imx6.c to newer file. And I patched these two points.

 

- LOW_ACTIVE

- if (imx6_pcie->ext_osc /*&& is_imx6qp_pcie(imx6_pcie)*/) {

to pci-imx6.c.

 

And I activated PCIe end point unit on FPGA.

I got that those messages were also displayed at not only when driver cannot input correct clock but when PCIe EP not connected . 

 

Thank you for your advice.

 

best regards,

0 Kudos
Reply
3,042 Views
massohy
Contributor II

I want set CCM_ANALOG_PLL_ENET to 0x00114000. But I checked that register after kernel booted, then it was 0x00017000. What file should I change for setting that register value before initializing pci driver.

0 Kudos
Reply