PCIe controller of i.MX8MM DMA transfer support

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

PCIe controller of i.MX8MM DMA transfer support

1,107件の閲覧回数
yasunori_suzuki
Contributor I

I have a question about PCIe controller of i.MX8MM.

Can  I use DMA transfer in RC mode?

Linux driver implemented DMA transfer in EP mode only.

But i.MX8MM reference manual seems like PCIe controller supports DMA tarnsfer RC mode and EP mode.  

BSP version is L4.14.98 2.00ga.

ラベル(1)
0 件の賞賛
返信
1 返信

1,026件の閲覧回数
weidong_sun
NXP TechSupport
NXP TechSupport

Hi 康議 鈴木,

According to the PCIe protocol, the DMA is initiated by the EP, and the RC side does not operate the DMA.

For example:

If I.MX8MM is used as EP, PCIe driver will operate DMA to transfer data.

Hope above information is helpful for you!

B.R,

Weidong