Hi,
I have a custom IMX6Q board in which I am not able to get PCIe up. I am using LTIB environment.
I have looked into other posts regarding the clock enable in RC mode, which seems to be enabled linux-3.0.35. I am trying to connect a dual port NIC card from Intel (0G174P) which is supported by the igb driver in kernel.
I always get this error during the kernel boot.
iMX6 PCIe PCIe RC mode imx_pcie_pltfm_probe entering.
PCIE: imx_pcie_pltfm_probe start link up.
link up failed, DB_R0:0x00d5f700, DB_R1:0x08200000!
IMX PCIe port: link down!
I had initially only connected PCIe RX, TX and CLK (driven by IMX6). I tried connecting a GPIO for PCI_Reset but that didn't help my cause.
Can you please suggest me what should I do next in order to get PCIe interface checked out?
~Raj
Hi Raj
you can try to connect in Gen1 mode:
How to force iMX6 PCIe into Gen 1 mode | Freescale Community
play with GPR8 PCIe phy levels IMX6DQRM sect.36.4.9 GPR (IOMUXC_GPR8)
if issue is caused by noise, one can try SDK example running it from OCRAM
i.MX 6Series Platform SDK
: Bare-metal SDK for the i.MX 6 series
iRAM (OCRAM) i.MX6 SDK Application
Also one can try to measure signals using
AN4784 AN4784: PCIe Certification Guide
Best regards
igor
Hi Igor,
I looked at your suggested links. I don't have access to to high end scopes mentioned in the PCIe Express application notes.
Though I hooked up a Differential probe on the clock lines (I have disabled the code which that stops the clock if linkup fails) and can see 100MHz +/-500mV at the the connector. I am using u-boot-2009 and kernel 3.0.35 and having gone through many of the links on the community, looks like reset to the PCIe card and clock enable is important. I don't see that correlated as of now.
Also I would like to understand do we get a similar error if the driver for a certain end point is not available at the kernel level?
Thanks
Raj
I think device should be detected, even there is no driver in kernel
Best regards
igor
Hi Igor,
I have tried multiple things on two different custom cards, but the PCIe link is still not up
In Gen 2 mode I get the debug register values DB_R0:0x00d53500, DB_R1:0x08200000, DB_RO data bit changes to 0x0037c800 by introducing some more delays in pcie_link_up function
When configured to Gen1 mode as per the link you shared the debug register values are DB_R0:0x00983800, DB_R1:0x08200000
I did not get what you meant by play with GPR8 PCIe phy levels, what values should I change and to what. If you would like to recommend some values that will be great.
I have made the reset to PCIe proper which gets enabled after the clock is enabled and stable.
Thanks
Raj
There was a link where someone faced similar issue and it seems got fixed with driver upgrade.
https://community.freescale.com/message/417588#417588
I will continue to look into the PCIe details further and see if init is not happening correctly.