PCIe Details of i.Mx6Q

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

PCIe Details of i.Mx6Q

546 Views
nanjundam
Contributor II

Hi,

I'm using i.Mx6Q (MCIMX6D6AVT10AD) in my design. The PCIe interface present with i.Mx6Q has no much explanation on the AC and DC characteristics (in the Datasheet & Reference manual).

Can anybody provide me the details ?

What is the standard of the PCIe signals , i.e. is it LVDS or HSCL standard ?

& What is the voltage level ?

Please help me with details.

Thanks & Regards,

Nanjunda M

Labels (3)
0 Kudos
Reply
1 Reply

415 Views
igorpadykov
NXP Employee
NXP Employee

HI Nanjunda

i.MX6 PCIe module complies with PCI Express Gen 2.0 specifications

which can be found on PCI SIG site

https://pcisig.com/specifications/pciexpress/base2/

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply