PCIE CLOCK GENERATOR

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

PCIE CLOCK GENERATOR

1,764 Views
HM_BDBA
Contributor I

Hello NXP Team

 

I have a query regarding PCIe clock generator used in 8MPLUS-BB Reference Board . 

As per reference board to use internal clock, (When using internal clock populate R135, R136, remove R131, R132, R137, R138) , Have NXP validated reference board with internal clock (clock sources by iMX 8M plus processor to peripheral, without using pcie clock generator) , Is that solution working ?

Do Pcie Clock Generator necessary for iMX 8M plus  ?

 

HM_BDBA_0-1651052625240.png

 

0 Kudos
Reply
2 Replies

1,727 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

On EVK, a PCIE clock generator chip (9FGV0241) is used to feed high-quality clock to both the PHY and connecter/device. If a PCIE clock generator is not available, use the internal clock of the chip. Note that the internal clock exhibits larger jitter than that from PCIE clock generator.

0 Kudos
Reply

1,748 Views
HM_BDBA
Contributor I

Hello NXP 

 

Please respond on this query. 

0 Kudos
Reply