PCI Express "phy never came up" with BSP 3.10.17

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

PCI Express "phy never came up" with BSP 3.10.17

553 Views
charleshuang
Senior Contributor II

I'm using BSP fsl-yocto-3.10.17_1.0.0 on imx6 dual

and I have a similar issue with these:

https://community.freescale.com/message/383712#383712

But I find two patches in

https://community.freescale.com/message/519666#519666

It works for "phy never came up" issue.

My question:

Is the issue caused by new-generation CPU ?

Labels (1)
Tags (2)
0 Kudos
1 Reply

394 Views
igorpadykov
NXP Employee
NXP Employee

HI charles

no, issue is not related to new-generation CPU,

processors remain the same. Patches adjust timings necessary for pcie

internal plls locking after warm-reset. In particular bit REF_SSP_EN

register GPR1 should be set only afer plls locking (it is not cleared

automatically after warm-reset).

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos