Hi,
I am using Sabresd Board i want to run "pci" command at u-boot for that i have added following lines to "mx6sabre_common.h".
#define CONFIG_CMD_PCI
#ifdef CONFIG_CMD_PCI
#define CONFIG_PCI
#define CONFIG_PCI_PNP
#define CONFIG_PCI_SCAN_SHOW
#define CONFIG_PCIE_IMX
#endif
but when i compile i am getting compilation errors as follows.
In function `imx_pcie_write_config' undefined reference to `_data_abort'
...
I want to know will sabresd boards support pci commands at u-boot?
if so what else i need to define to use pci commands?
 
					
				
		
 alejandrolozan1
		
			alejandrolozan1
		
		
		
		
		
		
		
		
	
			
		
		
			
					
		Hi,
Are you still getting the compiling errors?
Best Regards,
Alejandro
Hi Alejandro,
I have added those lines in my code still same errors i am getting.
Here are my error logs.
aisurya/saisurya/projects/VELU_WMSD/build/tmp/sysroots/imx6qsabresd/usr/lib/arm-poky-linux-gnueabi/4.8.2 -lgcc -Map u-boot.map -o u-boot
| drivers/pci/built-in.o: In function `imx_pcie_read_config':
| /home/saisurya/saisurya/projects/VELU_WMSD/build/tmp/work/imx6qsabresd-poky-linux-gnueabi/u-boot-fslc/v2014.01-r0/git/drivers/pci/pcie_imx.c:392: undefined reference to `_data_abort'
| drivers/pci/built-in.o: In function `imx_pcie_write_config':
| /home/saisurya/saisurya/projects/VELU_WMSD/build/tmp/work/imx6qsabresd-poky-linux-gnueabi/u-boot-fslc/v2014.01-r0/git/drivers/pci/pcie_imx.c:416: undefined reference to `_data_abort'
| make: *** [u-boot] Error 1
Hi Saisurya,
If you see the imx pcie driver "drivers/pci/pcie_imx.c", the definition of imx_pcie_fix_dabt_handler(bool set) says :
/*
* Replace the original ARM DABT handler with a simple jump-back one.
*
* The problem here is that if we have a PCIe bridge attached to this PCIe
* controller, but no PCIe device is connected to the bridges' downstream
* port, the attempt to read/write from/to the config space will produce
* a DABT. This is a behavior of the controller and can not be disabled
* unfortuatelly.
*
* To work around the problem, we backup the current DABT handler address
* and replace it with our own DABT handler, which only bounces right back
* into the code.
*/
Here, *_data_abort, is the backup handler and should be defined somewhere else as declared extern here.
I've also got the same issue and narrowed down by defining it global in u-boot/arch/arm/cpu/armv7/start.S file.
Just adding below line in the mentioned file(line no. 44) helped me. Hope, it'll work for you too.
.globl _data_abort
 
					
				
		
 fabio_estevam
		
			fabio_estevam
		
		
		
		
		
		
		
		
	
			
		
		
			
					
		Hi Saisurya,
2014.01 is a bit old. I would suggest you to use 2015.04 instead.
PCI works out of box in this version on mx6sabre.
Regards,
Fabio Estevam
 
					
				
		
 alejandrolozan1
		
			alejandrolozan1
		
		
		
		
		
		
		
		
	
			
		
		
			
					
		Hi,
Which configuration are you using? As far as I remember the mx6sabresd enables this option.
Have you tried this one?
Best Regards,
Alejandro
Hi,
I am unsing "include/configs/mx6sabresd.h" and mine was sabresd board.
 
					
				
		
 alejandrolozan1
		
			alejandrolozan1
		
		
		
		
		
		
		
		
	
			
		
		
			
					
		Hi,
Have you tried the version Fabio suggested?
/Alejandro
 
					
				
		
 alejandrolozan1
		
			alejandrolozan1
		
		
		
		
		
		
		
		
	
			
		
		
			
					
		I tried that config and I did not get any issue and I did not have to modify the mx6sabre_common.h file. Which BSP version are you using?
/Alejandro
 
					
				
		
 alejandrolozan1
		
			alejandrolozan1
		
		
		
		
		
		
		
		
	
			
		
		
			
					
		Hi,
I have this
#define CONFIG_CMD_PCI
#ifdef CONFIG_CMD_PCI
#define CONFIG_PCI
#define CONFIG_PCI_PNP
#define CONFIG_PCI_SCAN_SHOW
#define CONFIG_PCIE_IMX
#define CONFIG_PCIE_IMX_PERST_GPIO IMX_GPIO_NR(7, 12)
#define CONFIG_PCIE_IMX_POWER_GPIO IMX_GPIO_NR(3, 19)
#endif
in the include/configs/mx6sabresd.h file and it compiled with not problems.
/Alejandro