PCB of i.MX8M-EVK

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

PCB of i.MX8M-EVK

728 次查看
asou_junichi
Contributor I

Dear Support team,

PCB of i.MX8M-EVK is a 10-layer PCB.

Question.

Is it a through-hole PCB or a build-up PCB?

BR,

J.A

标签 (1)
0 项奖励
2 回复数

636 次查看
asou_junichi
Contributor I

Thank you for your answer.

I got it.

BR,

JA

0 项奖励

636 次查看
art
NXP Employee
NXP Employee

The PCB of the i.MX8M EVK board is the through-hole one.


Have a great day,
Artur

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励