PCA9450CHN for iMX8M Nano

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

PCA9450CHN for iMX8M Nano

1,391 次查看
paultran
Contributor I

hi,

Could you please help to advise that PCA9450CHN can be used for iMX8M Nano 

cause we have stock of PCA9450CHN and need to start a new design with iMX8M Nano, if possible 

- any SW config via i2c required 

- any application note for HW design 

Thanks 

标签 (2)
0 项奖励
回复
3 回复数

1,363 次查看
paultran
Contributor I

hi, Gouweisun 

Thanks for your reply, we understood that PCA9450B is the focus of iMX8 Nano 

but the question is: if we use PCA9450C for iMX8 Nano, is it possible? and any SW or HW config that we need to highlight 

following the spec, it can be done by not using the BUCK3. 

but imx8 and PCA9450C are communicated via i2c, so we need to check any SW configuration or not 

Thanks 

 

 

0 项奖励
回复

1,361 次查看
guoweisun
NXP TechSupport
NXP TechSupport

You need change dual phase configuration using two inductors instead of one, no need change for software side.

0 项奖励
回复

1,368 次查看
guoweisun
NXP TechSupport
NXP TechSupport

The reference design is used the PCA9450B.

IMX8MNLPD4EVKHUG.pdf

The different between PCA9450B and PCA9450C are:

1:PCA9450B – Two 3 A buck regulators
   PCA9450C – 6 A dual-phase buck regulator and 3 A buck regulator

2:

guoweisun_0-1683176306233.png

 

0 项奖励
回复