PCA9450CHN for iMX8M Nano

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

PCA9450CHN for iMX8M Nano

1,388 Views
paultran
Contributor I

hi,

Could you please help to advise that PCA9450CHN can be used for iMX8M Nano 

cause we have stock of PCA9450CHN and need to start a new design with iMX8M Nano, if possible 

- any SW config via i2c required 

- any application note for HW design 

Thanks 

Labels (2)
0 Kudos
Reply
3 Replies

1,360 Views
paultran
Contributor I

hi, Gouweisun 

Thanks for your reply, we understood that PCA9450B is the focus of iMX8 Nano 

but the question is: if we use PCA9450C for iMX8 Nano, is it possible? and any SW or HW config that we need to highlight 

following the spec, it can be done by not using the BUCK3. 

but imx8 and PCA9450C are communicated via i2c, so we need to check any SW configuration or not 

Thanks 

 

 

0 Kudos
Reply

1,358 Views
guoweisun
NXP TechSupport
NXP TechSupport

You need change dual phase configuration using two inductors instead of one, no need change for software side.

0 Kudos
Reply

1,365 Views
guoweisun
NXP TechSupport
NXP TechSupport

The reference design is used the PCA9450B.

IMX8MNLPD4EVKHUG.pdf

The different between PCA9450B and PCA9450C are:

1:PCA9450B – Two 3 A buck regulators
   PCA9450C – 6 A dual-phase buck regulator and 3 A buck regulator

2:

guoweisun_0-1683176306233.png

 

0 Kudos
Reply