PCA9450 pin connection when unused

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

PCA9450 pin connection when unused

1,142 Views
yuji_matsunami
Contributor II

Hello,

Could you please tell me the how connection of unused below pins ?

SCLL, SDAL, SCLH, SDAH

Thanks for your help.

Labels (2)
0 Kudos
4 Replies

1,139 Views
igorpadykov
NXP Employee
NXP Employee

Hi Yuji

 

they can be left unconnected. As described in sect.7.9 I2C level translator

Power management IC for i.MX 8M application processor family

"PCA9450 I2C Level translator is controlled by I2C register, CONFIG2 Reg. When it is
configured to disabled, all I/Os assume the high-impedance OFF-state."

 

Best regards
igor

0 Kudos

1,128 Views
yuji_matsunami
Contributor II

Dear igor-san,

I got it now,

also, Is the pull-down resistance not necessary to the CLK_32K_OUT pin ?
When there is no CLK output, does it become Hi-Z and cause malfunction due to noise?

Best Regards,
Yuji

0 Kudos

1,122 Views
igorpadykov
NXP Employee
NXP Employee

Hi Yuji

 

for CLK_32K_OUT please create new thread as this is new question.

 

Best regards
igor

0 Kudos

1,103 Views
yuji_matsunami
Contributor II

Thanks for your support.

0 Kudos